Article

A gamechanging monitor: designed for many, made only by us.

Nishant Nishant
computer monitor

A gamechanger? Well, yes. In our world of displays, it can be tempting to announce every new innovation with a huge fanfare and excitement. But the 23.1" Stretched In-Cell Monitor is genuinely going to be a huge deal for so many of our customers.

Why? One word: versatility. This is a product which has potential for so many applications and environments. It's a product that’s been designed to meet a multitude of needs across a number of industries:

  • A sleek design is ideal for retail, where eye-catching, ultra-wide displays are essential for digital signage, advertisements, and in-store promotions.
  • Its wide viewing angle makes it ideal for transportation hubs, to display real-time information at train stations and airports.
  • Durable construction makes sense for industrial and manufacturing environments, where it can display essential data, alerts, and operational information.
  • Attractive, dynamic displays are just what guests need in hospitality and entertainment venues, where it can be used for wayfinding, event schedules, and promotional content.

But let’s talk technical. After all, that’s what you’re here for. The 23.1" Stretched Monitor by Avnet Displays isn’t just a display; it's a comprehensive solution. It’s a monitor with in-cell touch technology, which integrates the touch sensor directly into the LCD cell. Besides making the monitor slicker and more attractive, this improves the responsiveness, accuracy and precision of the touch by reducing parallax. And the lack of an additional layer reduces reflection, increases brightness and aids clarity.

Uniquely, this monitor has an aspect ratio of 12.6:1 that you won’t find anywhere else and has an integrated system which combines a powerful quad-core CPU, sufficient memory, and Android OS – guaranteeing smooth and efficient operation. The 400 cd/m2 brightness and 3000:1 contrast ratio ensure that our monitor delivers exceptional clarity and visibility, outperforming others in the same category.

Key Features  
Panel Size: 23.1"
Display Ratio: 12.6:1
Resolution: 1920(V) x 158(H) at 83 PPI
Brightness: 400 cd/m2 (typical)
Contrast: 3000:1 (typical)
Viewing Angle: 89°/89°/89°/89° (typical)
Touch Screen: Optional In-Cell touch technology
Installation: Wall-mounted
Material: Metal housing for durability
Storage Temperature: -20℃ to 60℃
Working Temperature: 0℃ to 40℃
Humidity Range: 5% to 95% (storage), 10% to 85% (working)

Our Avnet Displays come in a range of form-factors and our display-experts are on hand to guide you in the creation of display or touch solutions that meet your requirements. Find out how Avnet Displays can propel your product innovation and get in touch today.

Contact a Display Solutions Expert

About Author

Nishant Nishant
Stefano Rosato, Director, Technical Touch Technology, Avnet

Stefano Rosato is director of technical touch technology in the Display Solutions team at Avnet. Ste...

Additional Information

Avnet’s Displays team solves product design challenges for OEMs looking to build the perfect display technology into their products. Our in-house team works directly with businesses to solve all the challenges of integrating a display into a product design, from tiny wearables to massive outdoor screens. We design, build and deliver display solutions all over the world for established household brand names and industry disruptors alike.  If you need a display designed and integrated into your product, our team is here to help. Get in touch today to tell us about your challenge.

Marketing Content Spots
Related Articles
Related Articles
digital display
Avnet Displays and SiS: delivering excellence together
By Stefano Rosato   -   2025年5月28日
We have an impeccable track record for giving our customers the very best displays. So, we’d like to introduce you to Silicon Integrated Systems (SiS), whose specialized firmware and hardware meets our every expectation – and yours.
A close-up shot of a rectangular black display with a dark gray screen, showing a thin black bezel and a visible orange ribbon cable on the bottom right, against a plain white background.
The same, but different: the new SimplePlus 6.95” twins
By Frank Ploenissen   -   2025年4月16日
The SimplePlus family just keeps growing – and this time we’re welcoming twins! By popular demand, we’re introducing two new 6.95” touch displays which might look similar on the surface but, like all twins, have quite different personalities.
Related Events
Related Events

No related events found