Article

Avnet and supplier partners demonstrate connected capabilities at Embedded World 2023

Philip Ling
IoT HVAC Air Pressure Monitoring Display
Avnet /IOTCONNECT powers this HVAC air pressure monitoring demonstration

/IOTCONNECT™ is Avnet’s solution accelerator software for developing, deploying and maintaining connected products in a scalable, fast, simple and secure way.

Embedded World 2023 is set for March 14-16 in Nuremburg, Germany. Visitors to the conference will see demonstrations featuring /IOTCONNECT at the following booths:

  • Microchip (Hall 3A, Booth 3A-443)
    • Microchip’s WFI32 showcasing Secure Device Management (SDM)
  • AWS (Hall 4, Booth 4-550)
    • AWS on /IOTCONNECT
  • Microchip (Hall 3A, Booth 3A-443)
    • /IOTCONNECT SDM on Microchip ATECC608 Trust&Go
  • Microsoft (Hall 4, Booth 4-410)
  • NXP (Hall 4A, Booth 4A-222)
    • Connected Tractor - Windows IoT 10 Enterprise with /IOTCONNECT running on i.MX8
  • Avnet Silica booth (Hall 3A, Booth 3A-111)
    • Demos include:
      • /IOTCONNECT running on STM32U5
      • Windows 10 IoT Enterprise with /IOTCONNECT running on i.MX8
  • EBV Elektronik (Hall 3A, Booth 3A-125)
    • AWS on /IOTCONNECT
    • IoTConnect on PSOC (see below)
  • Avnet Abacus (Hall 3A, Booth 3A-125)
    • /IOTCONNECT on Panasonic 9520

Visitors to these booths can dive deeper into the demos at the show. For example, the connected HVAC demonstrator combines pressure sensors from TE Connectivity with a Wi-Fi-enabled microcontroller development board from Microchip. Information from the sensors is collected by the microcontroller and processed using /IOTCONNECT software. The processed data is then passed to another /IOTCONNECT component running on the cloud platform. A web-based dashboard, also generated using /IOTCONNECT technology, allows the sensor data to be monitored and actions to be sent back to the board.

The demo on the EBV booth shows /IOTCONNECT running on a PSOC62S2 and Optiga Trust M secure element from Infineon. It integrates several sensors and connects to a cloud platform over Wi-Fi using a muRata Type 1LV module, which is based on Infineon’s CYW43012 chipset.

Lou Lutostanski, vice president of IoT, Avnet, said: “IoTConnect addresses two critical requirements in IoT. The first is development of secure, connected products using the limited resources found in endpoints. The second is accessing the massive capabilities offered by cloud platforms. Our unique technology does both, making it safer, faster and easier for OEMs to leverage the latest improvements in technology.”

/IOTCONNECT includes software components for both endpoints and cloud platforms. This creates a secure end-to-end connection that provides the fast and scalable way for OEMs to develop and deploy IoT solutions. /IOTCONNECT components run on the industry’s smallest microcontrollers and the largest cloud platforms from AWS and Microsoft Azure.

One of the key advantages of /IOTCONNECT is the abstraction it provides between an IoT endpoint application and cloud-based microservices. As an example, using /IOTCONNECT , OEMs can develop smart sensors that take advantage of the latest machine learning algorithms, without the huge development effort needed to implement AI at the edge or in the cloud. /IOTCONNECT also manages device provisioning, over-the-air updates, and the secure data path between the two points.

/IOTCONNECT application accelerators

An application accelerator, based on /IOTCONNECT , is a pre-packaged, pre-enabled suite of software components designed to get OEMs to market faster. It combines secure device management with dashboards to capture and present data from your endpoints. It provides a simple way to access advanced cloud-based features and add value to application without increasing time to market.

Avnet has already developed application accelerators for many end markets. These include smart agriculture, smart factories, the connected workplace, smart offices, factory automation and many more.

Each accelerator is pre-integrated and configured for an end-application and can be customized to meet an OEM’s specific requirements. The majority of functionality is already included, and, in some cases, little or no further development will be needed. This pre-configured approach significantly reduces the development effort and enables OEMs to move rapidly through the integration and test phases, and on to mass deployment.

Partnering with cloud platform providers

Avnet is now partnering with AWS and Microsoft to provide its /IOTCONNECT technology to OEMs using either platform. Together, AWS and Microsoft Azure capture the majority of the IoT cloud platform market. /IOTCONNECT integrates with both, giving OEMs the flexibility to use their preferred platform.

Avnet at Embedded World

Avnet will be represented by its European subsidiaries:

Avnet Abacus (Hall 3A, Booth 3A-125)
Avnet Abacus is Avnet's European distributor for interconnect, passive, electromechanical, power supply, energy storage, wireless and sensor products. Avnet Abacus will champion sustainability at this year’s event. Visit Embedded World 2023 for more information and a code for free entry.

Avnet Embedded & Witekio (Hall 1, Booth 1-510)
Avnet Embedded specialises in embedded boards, display solutions, software and IoT. Together with Witekio, Avnet's embedded software company, you can find out about the latest innovations, like the Open Standard Module (OSM), which will be on display. Find out more or book an appointment here: Embedded World.

Avnet Silica (Hall 3A, Booth 3A-111)
Avnet Silica will be focusing on Smart Industry, in partnership with leading supplies including AMD Xilinx, Microchip, Nordic Semiconductor, NXP, onsemi and STMicro. Get a free ticket to the show, courtesy of Avnet Silica, here: Embedded World 2023.

EBV Elektronik (Hall 3A, Booth 3A-125)
EBV represents many of the companies exhibiting at the show, including Broadcom, Infineon, Espressif, Power Integrations and Renesas. Learn more and get free entry at Embedded World 2023.

Farnell (Hall 3A, Booth 3A-519)
Farnell provides easy access to electronic solutions for students, makers and professionals. As well as featuring many leading suppliers on its linecard, Farnell also includes element14, an Avnet community where engineers of all kinds get together to exchange ideas and share their knowledge. Learn more here: Embedded World 2023.

About Author

Philip Ling
Philip Ling, Technical Content Manager, Corporate Marketing

Philip Ling is a Technical Content Manager with Avnet. He holds a post-graduate diploma in Advanced ...

Marketing Content Spots
Related Articles
Related Articles
batteries
The choice of energy harvesters for self-sustaining sensors
By Avnet Staff   -   2025年6月27日
PART 2: This article reviews advances in self-sustaining sensor nodes, focusing on innovative designs tackling intermittent energy and ultra-low-power challenges.
flower pots containing batteries
How energy harvesting underpins the self-sustaining IoT sensor node
By Avnet Staff   -   2025年6月27日
PART 1: This article reviews advances in self-sustaining sensor nodes, focusing on renewable energy harvesting integration and power management techniques.
Related Events
Related Events