Article

Behind the Datasheet: Vision systems

Philip Ling
documents
Find out what an Avnet engineer advises you to consider when selecting an image sensor for your application.

Image sensors are highly integrated devices, often with multiple operating modes and configuration parameters. Far from being a drop-in device, they need to be carefully integrated into the hardware, and require strong support from the system’s embedded software.

As with all system-level components, there needs to be a robust and flexible interface between the hardware and the software. This typically means using a driver: a software component that acts as the counterpart to the hardware element. The driver provides the system’s software a way to access the features of the hardware component. As such, drivers are often specific to a particular component, at least at some level.

Generic drivers can be used, and these do provide a good starting point for developers, particularly if the hardware component uses industry-standard interfaces. Drivers are often — not always — developed and provided by the hardware component manufacturer. To compound the issue, drivers are also normally specific to the operating system being used (if any).

One of the reasons why Linux is now so popular is because it comes with a lot of drivers. The community is also very good at developing and sharing drivers. Periodically, stable drivers may be integrated into the latest Linux distribution. If a Linux driver exists for the hardware component, it can save the engineering team a lot of time and effort.

This isn’t always obvious to developers when they begin the process of selecting an image sensor for their embedded vision application.

In this interview, Avnet Technical Marketing Engineer Mario Bergeron explains what engineers need to think about both before and after selecting an image sensor.

Video Player is loading.
Current Time 0:00
Duration 0:00
Loaded: 0%
Stream Type LIVE
Remaining Time 0:00
 
1x
    • Chapters
    • descriptions off, selected
    • captions off, selected

      About Author

      Philip Ling
      Philip Ling, Technical Content Manager, Corporate Marketing

      Philip Ling is a Technical Content Manager with Avnet. He holds a post-graduate diploma in Advanced ...

      Marketing Content Spots
      Related Articles
      Related Articles
      virtual reality headset
      Beyond the datasheet: The no-code route to MEMS-based machine learning at the edge
      By Philip Ling   -   January 17, 2025
      New MEMS sensors from STMicroelectronics integrate an innovative machine learning core, making it simpler to deploy machine language in many applications where motion detection is used. We take a look beyond the datasheet to see how it works.
      globe
      2025 supply chain insights you won’t get from a genAI chatbot
      By David Paulson   -   January 16, 2025
      What are the biggest risks and/or opportunities facing stakeholders across the high-tech supply chain in 2025? The greatest opportunities lie in the details others overlook.
      Related Events
      Related Events