Article

Colour, style and shape: the art of coverglass

Nishant Nishant
Coverglass on a display

How many times have you touched a glass screen today? Ten? Twenty? Thirty? More? Unless you’re actively monitoring your screen time, it’s barely even a consideration. But the kind of glass you interact with matters. The way it looks influences your experience of the screen, even if you don’t consciously realize it. And the coverglass has usually been designed for ease of use – and style.

You see, glass doesn’t have to be dull and square. It’s a beautifully adaptable material, and very tempting to work with. Designers love it for its elegance and the ease with which it can be machined into a desired shape. Plus, it can be printed with borders, symbols, indicators – neutral and functional, or colorful and fancy.

Designers can choose hardened glass materials and sandwich composites, which provide extra stability, protection and safety. Each glass may have different qualities of impact resistance and even coloration, which can affect where it may be used and how.  For example, medical settings demand pure colors, but a fitness machine may use tinted glass to hide the display when it’s not in use.

Glass shaping is usually achieved using CNC machines, which can create a world of free shapes, as well as, forging openings in the glass for buttons or cable feeds. Edge treatments, such as C-shaping, provide an attractive finish and also provide additional stability in the case of side impact. Most modern techniques even allow the 3D shaping of glass you might see these futuristic designs in car interiors, on the coverglass of a wristwatch, or even used as the front piece of a coffee machine.

Print can add function and design to a pure transparent glass substrate. Simple graphical elements can highlight the position or functions of embedded buttons or connectors. And full or semi-transparent print elements allow light indicators to shine through, providing essential alerts and other information. Clever printing techniques can even disguise the display behind – hiding it from view when inactive, and making it appear when on.

Regardless of your creative or functional choices, all glass printing must meet the requirements of its environment – whether that’s being fit for outdoor use without the print colors fading, scratch resistant or providing the finest nuances in colorations. This is good advice, not just for the print on glass, but the overall choice of materials and processes. With a vast number of functional and design options to choose from, it pays to work with an expert. Our specialists have all the necessary knowledge (and more!) to evaluate every use case presented to them and can help you to make the perfect glass selection for your product.

Our Avnet Displays come in a range of form-factors and our display-experts are on hand to guide you in the creation of display or touch solutions that meet your requirements. Find out how Avnet Displays can propel your product innovation and get in touch today.

Contact a Display Solutions Expert

About Author

Nishant Nishant
Frank Ploenissen , Marketing Manager Display Integration, Avnet

After getting his diploma in electrical engineering, Frank entered the world of display solution and...

Additional Information

Avnet’s Displays team solves product design challenges for OEMs looking to build the perfect display technology into their products. Our in-house team works directly with businesses to solve all the challenges of integrating a display into a product design, from tiny wearables to massive outdoor screens. We design, build and deliver display solutions all over the world for established household brand names and industry disruptors alike.  If you need a display designed and integrated into your product, our team is here to help. Get in touch today to tell us about your challenge.

Marketing Content Spots
Related Articles
Related Articles
A close-up shot of a rectangular black display with a dark gray screen, showing a thin black bezel and a visible orange ribbon cable on the bottom right, against a plain white background.
The same, but different: the new SimplePlus 6.95” twins
By Frank Ploenissen   -   April 16, 2025
The SimplePlus family just keeps growing – and this time we’re welcoming twins! By popular demand, we’re introducing two new 6.95” touch displays which might look similar on the surface but, like all twins, have quite different personalities.
flower on a screen
Transparently brilliant: the new Simple Plus Open Frame
By Stefano Rosato   -   April 3, 2025
Adaptable to any aesthetic or location, and ready for anything, our stunning new transparent OLED monitor, ‘Simple Plus Open Frame’, is so incredibly crystal clear, we can hardly take our eyes off it.
Related Events
Related Events

No related events found