Article

What is polarization, keying and color coding for interconnect?

Jamie Peterson
electric vehicle dashboard

Establishing a properly aligned connection quickly is key in any assembly or installation process.  Polarization, keying and color coding are primary means to ensuring connections are made quickly and safely.  In this article we’ll discuss each of these means and the advantages of them.

What is Keying?

Many connectors are designed with a means of being “keyed”, but what does this really mean and what is it designed for?  Keying is an important feature because it prevents mis-mating.  Incorrect mating could result in mechanical damage, lost signals, or even a short circuit, resulting in lost.  Resulting in lost time for troubleshooting and possibly damaged equipment.  Connector keying is the primary means of combating these situations by ensuring the connectors can only be mated in one direction.  Keying takes different forms such as a rectangular connector with a blanking pin in one position or a circular connector with a notch to ensure proper alignment of all pins such as the Molex BradPower D-Size connectors.

Polarization

Polarization preventss mis-mating by allowing only one orientation to connect which is especially important when the operator is unable to see the connector parts while uniting them, or “blind mating”.  The Molex polarized Saber Power connector ensures the proper orientation is easily achieved.  The image below illustrates how the shape of each position of the receptacle ensures proper polarization.

Color Coding

In a situation where there are several connectors that look similar, color coding helps the operator identify the proper connections quickly, saving time in the assembly or installation process.  Examples can be seen in common connectors such as the audio video RCA cables where red, white and yellow indicate right and left channel audio and video, or the Molex CP Wire to Board connectors where each color is for a specific signal or voltage.

Conclusion

All three of these concepts are relatively simple, but provide a crucial means of safety, speed and structure in assembly and installation.  While polarization and keying are commonly confused, you can see how each serves a specific purpose.  Keying can add bulk to a connector but provides a physical attribute, polarization ensures each contact is connected with the proper mate and color coding provides a quick visual indication for proper connection without adding bulk.

Our technical experts at Avnet are here to help you choose the right solution for your application.

 

About Author

Jamie Peterson
Jamie Pederson, Technical Content Manager

Jamie Pederson is a Technical Content Manager with Avnet. He has 18 years of electronics industry ex...

Marketing Content Spots
Related Content
Molex campaign, electric vehicle dashboard
 
 
Increased demand for ADAS and autonomous driving are pushing automakers to add more electronic control units and next-gen domain control units to vehicles resulting in a need for reliable interconnect solutions in harsh environments.
 
Related Articles
Related Articles
5G connectivity illustration
An introduction to mmWave connectors for 5G wireless networks
By Avnet Staff   -   July 16, 2024
Addressing the challenges of mmWave for 5G networks requires careful system design and mmWave RF connector selection to help maximize link range, ensure link reliability and protect signal integrity.
cityscape with radio waves
How to evaluate 5G mmWave Phased Array Antenna Modules
By Steven Fireman   -   May 29, 2024
Faster 5G development requires hardware and software with proven compatibility, plus precision instruments and interconnects to ensure the stability and accuracy of test and simulation results.
Related Events
Related Events
airplane cockpit looking out on the runway
More Electrification in Aircraft
Date: October 11, 2022
Location: Virtual
satellite in orbit
Space 2.0: AMD Technologies for New Space
Date: February 23, 2022
Location: Webinar