Article

关于5G系统的机电互连,你需要知道些什么

woman using mobile device in remote location

向设备提供5G的互连挑战

你可能感觉5G无处不在,但人们的共识是,最新的蜂窝网络仍然需要几年时间才能达到4G/LTE的普及水平。这符合每10年有一个新网络的历史趋势,我们可以预计6G系统将在2030年左右开始出现。这也使得现在以5G为目标的人都成为 "落后的早期使用者",一个听起来有点矛盾的说法。

这是件好事。早期的用户已经在那里,但还没有达到类似主流的程度。现在是开发第一代5G解决方案的好时机。制造商可以预期在6G开始接管市场之前,开发几代产品来跨越这十年。

任何第一代产品都是建立卓越设计的理想场所,它可以在遇到和克服与新技术相关的挑战时完成。对于5G,主要的挑战也是最大的特点:性能。5G来了,一切都会变快。设计师和系统工程师会立即明白,对他们来说,快速并不总是等于快乐。

对于任何高频信号来说,信号完整性是一个大问题,无论它是通过导体还是在空气中传播。5G的所有优势——比如高度密集的流量、更有效的频谱利用、更多的带宽和更低的延迟—— 都需要在网络中的每个点上实现。这包括在板级、板与板之间以及这些板上的组件之间。这就是4电平脉冲幅度调制(PAM-4)方案的重要性所在。它将提供56 Gbps和112 Gbps的速度,远远高于它所取代的不归零编码(NRZ)调制方案。虽然NRZ仍将使用一段时间,但PAM-4将使5G能够实现。


国际电信联盟ITU-R M.2083中定义的5G网络的关键能力。(来源:ETSI)

欧洲电信标准协会(ETSI)定义了5G系统必须满足的速度、延迟和效率的八个方面,如下所示。ETSI更加强调国际电信联盟无线电通信部门(ITU-R)确定的三个主要用例:增强型移动宽带(eMBB)、增强型机器类型通信(eMTc)和超可靠、低延迟通信(URLLC)。为了满足这些用例的要求,该行业正在利用新的技术和方法,如毫米波传输、更小和更多的单元、波束成形和MIMO天线技术。MIMO的性质增加了发射器中的天线密度,使天线阵列密度能高达256个单元。

从设备制造商的角度来看,这表明设备在物理上更小、更省电,但它们要处理更多的信号路径。这些”物理连接“需要极高的信号完整性,达到能够支持PAM-4传输速率的水平。预计,所有的垂直市场都会需要5G,主要是因为它的低延迟性。他们将依赖能够在组件层面支持该水平的吞吐量的系统。

新的网络

从4G/LTE转向5G的部分原因是,它重新定义了网络拓扑结构。前几代产品都是建立在传统系统上,延续了技术和方法。对于5G来说,这些遗留系统已经被搁置。这可以用5G所采用的新无线电标准为特征。实际上,网络的方方面面都被重新定义。当然,它必须在实现这一目标的同时,仍然在一定程度上依赖现有的技术,如能够承载毫米波信号的射频连接器。

5G开放性的提高,使网络结构发生了根本性变化。4G的无线接入网络(RAN)包括一个基带单元和远程无线电头。在5G中,这已成为由集中式单元、分布式单元、无线电单元和MIMO天线组成的前传网络(fronthaul network)。

这就是部署新的远程无线电单元、有源天线单元和基带单元的地方。前传网络将连接到核心网络,而前面概述的用例中的实际设备将使用MIMO天线通过前传网络连接。

虽然光纤互连将在整个网络的许多地方使用,但铜质互连在新的5G拓扑结构中仍有重要作用。

Molex莫仕全球产品经理Mike Hansen解释说,对铜质互连解决方案的主要需求是在电路板之间布线,有趣的是,也包括跨板布线。使用带双轴的电缆组件可以在避免与PCB导线相关的损失的同时,实现高速信号的传输。

Hansen介绍说,随着有源天线单元(AAUs)的发展,5G已经创造了一个转变。这些AAU的特点是大规模MIMO架构和大量的处理,都在一个非常小的区域内。在系统架构中,高密度的铜质互连是必不可少的。

输送高速5G信号

在电路板层面,PCB正成为高速信号的一个主要障碍。虽然转向光纤互连可以消除部分痛苦,但在某些时候,电信号仍然需要与集成电路接口。这时,先进的互连解决方案可以提供更高的信号完整性,和敏感的差分信号(Differential Signal)所需的较低插入损耗。

改进的边缘连接器提供了除电源之外,在单个高度紧凑的连接器上挤压和差分对(differential pairs)和单端信号所需的密度。在实现这一点的同时,还能避免信号完整性问题。

现在,信号不再在拥挤和有损耗的PCB上布线,而是使用双同轴电缆制成的组件从PCB的一侧布线到另一侧,或直接从I/O到集成电路。这些所谓的旁路电缆组件避免了与传统PCB相关的损失,而不需要进出光域,使成本和延迟降到最低。

为了支持5G网络所涉及的带宽,运营商正在使用56 Gbps的PAM-4信令,并在可能的情况下使用112 Gbps。这种速度的信号路由有赖于连接器层面上的精细阻抗匹配。用于路由PAM-4信号的解决方案包括Molex的NearStack 100欧姆和85欧姆系列。NearStack PCIe连接器支持NRZ编码的32 Gbps。

更激进的解决方案,如NearStack On-the-Substrate系统,使用直接到芯片基板的双轴连接,将接触点直接放在ASIC的表面。该系统目前支持56 Gbps和112 Gbps的PAM-4连接。


Twinax电缆组件允许敏感的高速差分信号直接从I/O到ASIC,而不会产生与PCB中FR4轨道相关的损失。(来源:Molex)

欲了解更多产品信息,请在专题页面供应商列表中下载查看5G系列产品白皮书。

浏览更多 

Marketing Content Spots
Two businessmen shaking hands in an office setting
 
 
From the interconnect design challenges of 5G to preparing now for 6G, what will it take to build the networks of the future to enable your vision? Explore the key characteristics of almost limitless connectivity in any context.
 
Related Articles
Related Articles
A collage of thermal management technologies
Thermal innovations keep high-performance electronics cool
By Avnet Staff   -   2025年4月4日
Thermal management solutions are innovating rapidly to address the challenge of keeping electronic systems cool as they get smaller and faster, oftentimes used in combination to spread and transfer the heat.
connectors in rain
Connectors for harsh environments
By Avnet Staff   -   2025年4月2日
The right connectivity solution for harsh environments depends on an understanding of the disruptive environmental factors and how they affect sensitive equipment. With this knowledge, engineers can select connectors
Related Events
Related Events
satellite in orbit
Space 2.0: AMD Technologies for New Space
Date: 2022年2月23日
Location: Webinar