The future of the Internet of Things means billions of devices must communicate with servers on the internet, and with each other. Security and connectivity will be paramount. Explore our resources to stay up to date with security and connectivity trends and technology.
Bluetooth 6.0 comes with six new features of note. With centimeter-level positioning one of them and now available, will this change the way we navigate?
OEMs and start-ups are paying attention to a development that places cellular and satellite technologies on a path to convergence. The growth of connected devices and associated traffic blurs the line between satellite and terrestrial networks.
Faster 5G development requires hardware and software with proven compatibility, plus precision instruments and interconnects to ensure the stability and accuracy of test and simulation results.
10BASE-T1S Ethernet is the perfect protocol for implementing zonal electronic and electrical architectures in automobiles. This article highlights how it meets automotive requirements and showcases the Onsemi product family.
Are you tempted to take an engineering shortcut in your next design? Take one supplier partner engineer’s experience and advice that there’s an excellent chance it will come back and bite you.
Establishing a properly aligned connection quickly is key in any assembly or installation process. Polarization, keying and color coding are primary means to ensuring connections are made quickly and safely. In this article we’ll discuss each of
A standing wave occurs when the reflected signal is in phase with the source. When it happens in a transmission line, it is normally unwanted because it results in emitted radiation. However, it is exactly that radiation that maximizes the signal’s streng...
As households replace cable with streaming services, can OTA TV still compete? Many say yes. Although it operates at the same frequencies as existing channels and access remains free, the true benefits lie in NextGen TV’s hybrid architecture.
Your industrial environment is a complex network of devices with varying roles and responsibilities. Bringing all that together requires the application of proven and new technologies. Efforts are underway to make them all work in harmony.
From improved timing algorithms and sleep modes to the modernization of network hardware and new network protocols, 5G employs several power reduction strategies to manage network energy consumption.
A recent survey found 99 percent of respondents identified networking challenges as their customers’ primary roadblock to Industrial IoT implementation. Can cellular networks replace conventional networks for IIoT applications?
Avnet spoke with Molex Global Product Manager Mike Hansen about the role copper interconnect is playing in the development of the next high-speed cellular network.
High-performance radio frequency, input/output and board connectors are helping developers meet the challenge of 5G. Designed for mmWave and PAM-4 signals in the fronthaul of the network, engineers can use them to improve signal integrity.
5G will require a new network design in which smart repeaters, advanced software and algorithms, digital beamforming, and other techniques allow millimeter-wave signals to permeate RF-restrictive environments.
5G is a technological moving target. If designers had to rely only on hardware to make those changes, it’s possible that 5G would be far too expensive or technically impossible to deploy. That’s where SDR comes in.
Work on 6G is already underway to define what the standard will do and how it will do it. If 5G is about enabling the Internet of Things (IoT), 6G is about enabling the Internet of Everything – including you.
The flat CAN bus architecture is obsolete. We’ll see major changes over the next 10-15 years, but let’s look even further. NXP has forecasts as far out as 2050 and we can use those to gain an inkling of what IVN will look like in 30 years.
In-vehicle networking (IVN) is experiencing strong growth due to the increase of complex capabilities in next-generation transportation applications and the rapid advancement of technology.
The CAN bus has served the industry for over three decades, and now Ethernet is moving in. While it’s not perfect for everything, CAN still has gas left in the tank.
To keep up with the demand for more processing power and blazing-fast data transmission speeds, the auto industry is moving toward a zonal electronic/electrical (E/E) architecture.
Learn how LoRaWAN and artificial intelligence (AI) at the edge can revolutionize the internet of things by reducing data transmission and improving latency.
Development of very low powered analog body sensors, digital microcontrollers, and innovative power and battery management circuits are driving the growth of wearable healthcare products.
When you think of experiencing music, what comes to mind? The sound. But sound is vibrations—and the key to how Avnet created a wearable to allow deaf and hard of hearing people to listen to live music.