The best power converters are not always the ones that switch the fastest. Gallium Nitride (GaN) switches faster than other power transistors, but sometimes it is too fast. Silicon Carbide (SiC) MOSFETs may sometimes be a better option.
While silicon served us admirably for half a century, engineers are turning to wide bandgap technologies such as silicon carbide and gallium nitride to increase converter/inverter efficiency as momentum to harness renewable energy increases.
Within EV fast charging technologies, focus is on the crucial role of DC-DC converters in enabling efficient energy transfer. The design will be influenced by the primary commercial objective.
As the EV charging infrastructure grows, EVSE providers need to offer a choice. Cost, efficiency and reliability are trade-offs that begin at the component level and move quickly to the converter topology.
The best power converters are not always the ones that switch the fastest. Gallium Nitride (GaN) switches faster than other power transistors, but sometimes it is too fast. Silicon Carbide (SiC) MOSFETs may sometimes be a better option.
The public image of silicon carbide (SiC) and gallium nitride (GaN) is as wonder materials. We know they are displacing older silicon technology, boosting the efficiency of power conversion stages. However, neither is a universal solution.
Depending on the design, wide bandgap devices may provide efficiency gains in power conversion for onboard chargers. But which do you choose over silicon if any? We look at the options and offer some advice.
SiC will soon overtake Si as the dominant semiconductor material for power devices with voltage rating higher than 600V. Designers looking to stay competitive and lower long-term system costs are turning to SiC-based technologies good reason.
While silicon served us admirably for half a century, engineers are turning to wide bandgap technologies such as silicon carbide and gallium nitride to increase converter/inverter efficiency as momentum to harness renewable energy increases.
Silicon carbide builds on established manufacturing methodologies but requires entirely new manufacturing processes. Increasing yield and reducing costs relies on imposing the highest quality at every stage.
SiC semiconductors are becoming ubiquitous in power conversion equipment, particularly in the areas of EVs, solar and energy storage systems. This article reviews applications and explores the figures of merit that can be used to compare devices.
In high reliability/availability applications, SiC semiconductors are seen as emerging technology. This article explains their benefits and how an end-to-end supply chain with robust testing makes SiC a safe design option.
SiC and GaN wide bandgap semiconductor switches can provide a step improvement in efficiency in power converters. Engineers should be aware that they have different secondary characteristics compared with Si-MOSFETS and IGBTs.
When it comes to smart control applications, it’s worth taking a step back to consider when and if the switch to wide bandgap from MOSFET or IGBT makes sense. When the answer is yes, then the decision is whether SiC or GaN is the way to go.
Even with the undeniable performance and potential of silicon carbide (SiC) technology, some designers may be hesitant initially to tackle new projects using SiC.