Custom Meta Tags
Category Attributes
Category Attributes
宽禁带技术   筛选条件   宽禁带技术 RSS FEED
宽禁带技术的实际应用已经达到了临界点,它的作用和功效不可否认。无论你是在探索碳化硅(SiC)还是氮化镓(GaN)电源解决方案,都可深入了解安富利关于宽禁带技术不断发展中的最新信息。
Wide bandgap semiconductor material in its raw form
When GaN is too fast for your application, consider SiC instead
By Avnet Staff   -   2023年4月24日
The best power converters are not always the ones that switch the fastest. Gallium Nitride (GaN) switches faster than other power transistors, but sometimes it is too fast. Silicon Carbide (SiC) MOSFETs may sometimes be a better option.
hand reaching out
您知道碳化硅品质优值(Figures of Merit)的重要性吗
2022年10月15日
碳化硅半导体在电力转换设备中越来越普遍,特别是在电动汽车、太阳能和储能系统领域。本文回顾了它的各种应用,并探讨可用于器件比较的碳化硅品质优值(Figures of Merit)。
ocean windfarm
How wide bandgap semiconductors are improving renewable energy design
2022年7月13日
While silicon served us admirably for half a century, engineers are turning to wide bandgap technologies such as silicon carbide and gallium nitride to increase converter/inverter efficiency as momentum to harness renewable energy increases.
two buisiness people exchanging handshake with SiC icons overlayed
近距离观测碳化硅的质量
2022年6月27日
碳化硅以既定的制造方法为基础,但需要全新的制造工艺。提高产量和降低成本取决于在每一阶段都实现最高质量。
mand holding testing equipment
鲁棒性测试对碳化硅供应链来说不可或缺
2022年6月10日
在高可靠性/可用性应用中,碳化硅半导体被视为新兴技术。本文解释了它们的优点,以及具有强大测试的端到端供应链如何使SiC成为安全的设计选项。
circuit board
使用宽带隙器件做电路设计时的注意事项
By Milan Ivkovic   -   2022年5月30日
碳化硅和氮化镓宽带隙半导体开关可以为功率转换器的能效带来进一步的提高。工程师应该知道,与Si-MOSFETS 和IGBT 相比,它们具有不同的次级特性。
WBG motor control
针对电机控制应用选择宽带隙器件
By Milan Ivkovic   -   2022年5月30日
当涉及智能控制应用时,我们需要冷静考虑是否从MOSFET或IGBT转换到宽带隙器件更有意义。如果答案是肯定的,那么方能决定采用碳化硅还是氮化镓。
woman navigating a smart car dash pad
车用宽带隙半导体正在前进
By Jason Struble   -   2021年8月24日
看看老一代硅基IGBT和MOSFET与新一代碳化硅开关之间的技术和成本比较。
Cleanroom tech with wafer
借助 SiC 技术,实现三大设计自由
By Milan Ivkovic   -   2021年4月17日
尽管 SiC 技术的性能和潜力毋庸置疑,但一些设计人员最初可能仍然会犹豫不决,无法下定决心使用 SiC 技术来处理新项目
lab techicians
The undeniable advantages of SiC technology over Si
By Milan Ivkovic   -   2021年4月16日
Silicon carbide (SiC) technology has reached the tipping point, the state when undeniable advantages push a technology into rapid adoption.
First1 Last  Results Per Page: 30 6090All      
Category Attributes
Training & Events
No related Training & Events found
Category Attributes
宽禁带技术   Filter By   宽禁带技术 RSS FEED
宽禁带技术的实际应用已经达到了临界点,它的作用和功效不可否认。无论你是在探索碳化硅(SiC)还是氮化镓(GaN)电源解决方案,都可深入了解安富利关于宽禁带技术不断发展中的最新信息。
EV car at charger
Understanding trade-offs for DC-DC converters in EV charging
By Avnet Staff   -   2024年6月24日
Within EV fast charging technologies, focus is on the crucial role of DC-DC converters in enabling efficient energy transfer. The design will be influenced by the primary commercial objective.
EV Power Supply
Designing Vienna Rectifiers for EV Chargers
By Avnet Staff   -   2024年6月24日
As the EV charging infrastructure grows, EVSE providers need to offer a choice. Cost, efficiency and reliability are trade-offs that begin at the component level and move quickly to the converter topology.
Wide bandgap semiconductor material in its raw form
When GaN is too fast for your application, consider SiC instead
By Avnet Staff   -   2023年4月24日
The best power converters are not always the ones that switch the fastest. Gallium Nitride (GaN) switches faster than other power transistors, but sometimes it is too fast. Silicon Carbide (SiC) MOSFETs may sometimes be a better option.
two materials combined in organic form
Combining GaN and SiC for cost-effective power conversion
By Avnet Staff   -   2023年4月20日
The public image of silicon carbide (SiC) and gallium nitride (GaN) is as wonder materials. We know they are displacing older silicon technology, boosting the efficiency of power conversion stages. However, neither is a universal solution.
A close-up of an onboard charger in an electric vehicle
Understand practical GaN and SiC differences for EV onboard chargers
By Avnet Staff   -   2023年4月18日
Depending on the design, wide bandgap devices may provide efficiency gains in power conversion for onboard chargers. But which do you choose over silicon if any? We look at the options and offer some advice.
Lab technicians in clean room
The undeniable advantages of SiC technology over Si
By Milan Ivkovic   -   2022年12月5日
SiC will soon overtake Si as the dominant semiconductor material for power devices with voltage rating higher than 600V. Designers looking to stay competitive and lower long-term system costs are turning to SiC-based technologies good reason.
ocean windfarm
How wide bandgap semiconductors are improving renewable energy design
2022年7月13日
While silicon served us admirably for half a century, engineers are turning to wide bandgap technologies such as silicon carbide and gallium nitride to increase converter/inverter efficiency as momentum to harness renewable energy increases.
two buisiness people exchanging handshake with SiC icons overlayed
A closer look at SiC quality
2022年6月27日
Silicon carbide builds on established manufacturing methodologies but requires entirely new manufacturing processes. Increasing yield and reducing costs relies on imposing the highest quality at every stage.
hand reaching out
Why you should care about SiC figures of merit
2022年6月10日
SiC semiconductors are becoming ubiquitous in power conversion equipment, particularly in the areas of EVs, solar and energy storage systems. This article reviews applications and explores the figures of merit that can be used to compare devices.
mand holding testing equipment
How robust testing forms part of the SiC supply chain
2022年6月10日
In high reliability/availability applications, SiC semiconductors are seen as emerging technology. This article explains their benefits and how an end-to-end supply chain with robust testing makes SiC a safe design option.
circuit board
Considerations when designing with wide bandgap devices
By   -   2021年12月20日
SiC and GaN wide bandgap semiconductor switches can provide a step improvement in efficiency in power converters. Engineers should be aware that they have different secondary characteristics compared with Si-MOSFETS and IGBTs.
WBG motor control
Selecting wide bandgap devices for motor control applications
By Milan Ivkovic   -   2021年12月20日
When it comes to smart control applications, it’s worth taking a step back to consider when and if the switch to wide bandgap from MOSFET or IGBT makes sense. When the answer is yes, then the decision is whether SiC or GaN is the way to go.
woman navigating a smart car dash pad
Advances in wide-bandgap semiconductors for vehicles
By Jason Struble   -   2021年8月24日
See the technical and cost comparisons between older silicon IGBT and MOSFET technologies and newer generation silicon carbide switches.
electric vehicle charging station sign
EV charging: The drive for faster charging speeds and higher efficiency
2021年8月11日
Fast DC chargers and wide-bandgap silicon carbide switches are key to improved EV charging.
Cleanroom tech with wafer
Three design freedoms enabled by SiC technology
By Milan Ivkovic   -   2021年4月17日
Even with the undeniable performance and potential of silicon carbide (SiC) technology, some designers may be hesitant initially to tackle new projects using SiC.
First1 Last  Results Per Page: 30 6090All