Custom Meta Tags
Category Attributes
Category Attributes
Category Attributes
Training & Events
No related Training & Events found
Category Attributes

Wide bandgap

  Filter By   Wide bandgap RSS FEED
Adoption of wide bandgap technology has reached the tipping point, and its usefulness is now undeniable. Whether you’re exploring silicon carbide (SiC) or gallium nitride (GaN) power solutions, dive into the latest information from Avnet on these evolving technologies.
EV car at charger
Understanding trade-offs for DC-DC converters in EV charging
By Avnet Staff   -   June 24, 2024
Within EV fast charging technologies, focus is on the crucial role of DC-DC converters in enabling efficient energy transfer. The design will be influenced by the primary commercial objective.
EV Power Supply
Designing Vienna Rectifiers for EV Chargers
By Avnet Staff   -   June 24, 2024
As the EV charging infrastructure grows, EVSE providers need to offer a choice. Cost, efficiency and reliability are trade-offs that begin at the component level and move quickly to the converter topology.
Wide bandgap semiconductor material in its raw form
When GaN is too fast for your application, consider SiC instead
By Avnet Staff   -   April 24, 2023
The best power converters are not always the ones that switch the fastest. Gallium Nitride (GaN) switches faster than other power transistors, but sometimes it is too fast. Silicon Carbide (SiC) MOSFETs may sometimes be a better option.
two materials combined in organic form
Combining GaN and SiC for cost-effective power conversion
By Avnet Staff   -   April 20, 2023
The public image of silicon carbide (SiC) and gallium nitride (GaN) is as wonder materials. We know they are displacing older silicon technology, boosting the efficiency of power conversion stages. However, neither is a universal solution.
A close-up of an onboard charger in an electric vehicle
Understand practical GaN and SiC differences for EV onboard chargers
By Avnet Staff   -   April 18, 2023
Depending on the design, wide bandgap devices may provide efficiency gains in power conversion for onboard chargers. But which do you choose over silicon if any? We look at the options and offer some advice.
Lab technicians in clean room
The undeniable advantages of SiC technology over Si
By Milan Ivkovic   -   December 5, 2022
SiC will soon overtake Si as the dominant semiconductor material for power devices with voltage rating higher than 600V. Designers looking to stay competitive and lower long-term system costs are turning to SiC-based technologies good reason.
ocean windfarm
How wide bandgap semiconductors are improving renewable energy design
July 13, 2022
While silicon served us admirably for half a century, engineers are turning to wide bandgap technologies such as silicon carbide and gallium nitride to increase converter/inverter efficiency as momentum to harness renewable energy increases.
two buisiness people exchanging handshake with SiC icons overlayed
A closer look at SiC quality
June 27, 2022
Silicon carbide builds on established manufacturing methodologies but requires entirely new manufacturing processes. Increasing yield and reducing costs relies on imposing the highest quality at every stage.
hand reaching out
Why you should care about SiC figures of merit
June 10, 2022
SiC semiconductors are becoming ubiquitous in power conversion equipment, particularly in the areas of EVs, solar and energy storage systems. This article reviews applications and explores the figures of merit that can be used to compare devices.
mand holding testing equipment
How robust testing forms part of the SiC supply chain
June 10, 2022
In high reliability/availability applications, SiC semiconductors are seen as emerging technology. This article explains their benefits and how an end-to-end supply chain with robust testing makes SiC a safe design option.
circuit board
Considerations when designing with wide bandgap devices
By   -   December 20, 2021
SiC and GaN wide bandgap semiconductor switches can provide a step improvement in efficiency in power converters. Engineers should be aware that they have different secondary characteristics compared with Si-MOSFETS and IGBTs.
WBG motor control
Selecting wide bandgap devices for motor control applications
By Milan Ivkovic   -   December 20, 2021
When it comes to smart control applications, it’s worth taking a step back to consider when and if the switch to wide bandgap from MOSFET or IGBT makes sense. When the answer is yes, then the decision is whether SiC or GaN is the way to go.
woman navigating a smart car dash pad
Advances in wide-bandgap semiconductors for vehicles
By Jason Struble   -   August 24, 2021
See the technical and cost comparisons between older silicon IGBT and MOSFET technologies and newer generation silicon carbide switches.
electric vehicle charging station sign
EV charging: The drive for faster charging speeds and higher efficiency
August 11, 2021
Fast DC chargers and wide-bandgap silicon carbide switches are key to improved EV charging.
Cleanroom tech with wafer
Three design freedoms enabled by SiC technology
By Milan Ivkovic   -   April 17, 2021
Even with the undeniable performance and potential of silicon carbide (SiC) technology, some designers may be hesitant initially to tackle new projects using SiC.
First1 Last  Results Per Page: 30 6090All