Custom Meta Tags
Milan Ivkovic

About Author

Ripal Vyas Headshot
Milan Ivkovic - Segment Director at EBV Elektronik, an Avnet Company

Segment Director

More From Author
Lab technicians in clean room
The undeniable advantages of SiC technology over Si
By Milan Ivkovic   -   2022年12月5日
SiC will soon overtake Si as the dominant semiconductor material for power devices with voltage rating higher than 600V. Designers looking to stay competitive and lower long-term system costs are turning to SiC-based technologies good reason.
WBG motor control
Selecting wide bandgap devices for motor control applications
By Milan Ivkovic   -   2021年12月20日
When it comes to smart control applications, it’s worth taking a step back to consider when and if the switch to wide bandgap from MOSFET or IGBT makes sense. When the answer is yes, then the decision is whether SiC or GaN is the way to go.
Cleanroom tech with wafer
Three design freedoms enabled by SiC technology
By Milan Ivkovic   -   2021年4月17日
Even with the undeniable performance and potential of silicon carbide (SiC) technology, some designers may be hesitant initially to tackle new projects using SiC.
Silicon carbide (SiC) and Gallium nitride (GaN)
The substantial benefits of silicon carbide (SiC) and gallium nitride (GaN) in power electronics
By Milan Ivkovic   -   2021年3月8日
Silicon carbide (SiC) and gallium nitride (GaN) are two semiconductor materials that are creating a significant shift in the power electronics market.