Colour, style and shape: the art of coverglass | Avnet Silica
Colour, style and shape: the art of coverglass | Avnet Silica

Colour, style and shape: the art of coverglass

Nishant Nishant
Coverglass on a display

How many times have you touched a glass screen today? Ten? Twenty? Thirty? More? Unless you’re actively monitoring your screen time, it’s barely even a consideration. But the kind of glass you interact with matters. The way it looks influences your experience of the screen, even if you don’t consciously realize it. And the coverglass has usually been designed for ease of use – and style.

You see, glass doesn’t have to be dull and square. It’s a beautifully adaptable material, and very tempting to work with. Designers love it for its elegance and the ease with which it can be machined into a desired shape. Plus, it can be printed with borders, symbols, indicators – neutral and functional, or colorful and fancy.

Designers can choose hardened glass materials and sandwich composites, which provide extra stability, protection and safety. Each glass may have different qualities of impact resistance and even coloration, which can affect where it may be used and how.  For example, medical settings demand pure colors, but a fitness machine may use tinted glass to hide the display when it’s not in use.

Glass shaping is usually achieved using CNC machines, which can create a world of free shapes, as well as, forging openings in the glass for buttons or cable feeds. Edge treatments, such as C-shaping, provide an attractive finish and also provide additional stability in the case of side impact. Most modern techniques even allow the 3D shaping of glass you might see these futuristic designs in car interiors, on the coverglass of a wristwatch, or even used as the front piece of a coffee machine.

Print can add function and design to a pure transparent glass substrate. Simple graphical elements can highlight the position or functions of embedded buttons or connectors. And full or semi-transparent print elements allow light indicators to shine through, providing essential alerts and other information. Clever printing techniques can even disguise the display behind – hiding it from view when inactive, and making it appear when on.

Regardless of your creative or functional choices, all glass printing must meet the requirements of its environment – whether that’s being fit for outdoor use without the print colors fading, scratch resistant or providing the finest nuances in colorations. This is good advice, not just for the print on glass, but the overall choice of materials and processes. With a vast number of functional and design options to choose from, it pays to work with an expert. Our specialists have all the necessary knowledge (and more!) to evaluate every use case presented to them and can help you to make the perfect glass selection for your product.

 

About Author

Nishant Nishant
Avnet Staff

We use Avnet Staff as a collective byline when our team of editors and writers collaborate on the co...

Colour, style and shape: the art of coverglass | Avnet Silica
Colour, style and shape: the art of coverglass | Avnet Silica
Related Articles
Display backlight system
Bright, brighter, brightest? Why a display backlight system is more than meets the eye
By Avnet Staff   -   2024年6月27日
The human eye doesn’t perceive light in a linear way. So, if you’re looking to achieve a super-bright result, your display will need a huge amount of energy – in fact, more than double the cost of a standard display.
Person using a tablet
ePaper integration with PCAP
By Avnet Staff   -   2024年6月27日
Electronic paper (also known as e-ink, electrophoretic display, or electronic ink) is a kind of electronic display that mimics the appearance of ink on paper.
Colour, style and shape: the art of coverglass | Avnet Silica
Related Events

No related events found

Related Designs Menu