EV Charging: How V2G Benefits Drivers and Electricity Suppliers
EV Charging: How V2G Benefits Drivers and Electricity Suppliers

EV Charging Series, Part 3: How V2G Benefits Drivers and Electricity Suppliers

Harvey Wilson, Technology Specialist Connectivity EMEA
Vehicle to Grid EV charging

Vehicle-to-grid (V2G) is the capability for EVs to send power from their batteries back to the main electricity grid. This can be hugely helpful in meeting demands on the grid, stabilising it, and dealing with the inconsistency of renewables. However, it brings with it new technical and commercial challenges and has been slow to find wide adoption.

Vehicle-to-grid has been a well-known concept since the 1990s when electric vehicles (EVs) seemed poised to become mainstream. However, the electric car revolution was delayed, and V2G's progress stalled before it even began – there simply weren't enough EVs on the road[1]

It was only in the 2010s and 2020s that higher sales of EVs put V2G back in the game as a viable technology. With a growing proportion of our electricity being generated by renewables, the storage and grid-balancing capabilities offered by V2G are coming at just the right time to help utilities manage their increasingly complex systems.

Renewables are unpredictable, so we need a way to store excess energy generated when the wind blows and the sun shines. This enables the grid to have spare energy available to handle short-term peak demands without having to keep costly gas and coal power plants available for occasional use.

However, storing electricity is surprisingly difficult and expensive. Home storage batteries, such as Tesla's Powerwall, would do the job, but they are a costly solution.

Instead, how about utilising all the batteries already sitting in our driveways?

Vehicles as energy stores

Using an EV battery to provide electricity to the grid may seem obvious, but it requires the right technology – specifically, the provision of bi-directional charging capability in both the charger and the car.

To ensure interoperability across multiple vendors, the ISO 15118 standard for communication between EVs and charging stations includes specifications for bi-directional charging. Currently, only EVs built to the CHAdeMO charging standard (developed by Japanese carmakers) can handle bi-directional charging [2], although efforts are underway to add this capability to other standards such as CCS.

While our primary focus in this article is on V2G, there is also ongoing interest in vehicle-to-home (V2H) and vehicle-to-load (V2L), often collectively referred to as V2X.

V2L enables a vehicle's battery to power electric devices, such as power tools or lights. V2H allows an EV battery to be used to power the home, ensuring the lights stay on during a power outage or storing power from home solar cells for later household use.

The benefits of V2G

Electricity at night is typically much cheaper than during the day due to considerably lower demand. Charging electric vehicles (EVs) overnight can save car owners a significant amount of money.

Moreover, the reduced demand at night means that a larger proportion of the electricity used for charging comes from renewable sources, as opposed to fossil fuel power plants that may only be activated during peak times. This contributes to utilities' efforts to lower carbon emissions.

In addition to assisting electricity suppliers in managing peak demands, the energy stored in EV batteries can also help them handle voltage and frequency fluctuations on the grid.

Given the unpredictable nature of renewables, instances of cheap electricity may arise with little notice, such as unexpected windy weather. The V2G system, including any consumer-facing applications, must be flexible enough to respond promptly. EV batteries are well-suited to serve as a nearly instant source of power, available more quickly than activating other power generators.

EV Charging home garage

Commercial issues

While the technology challenges of V2G are well on the way to being solved, the barriers to its adoption are now primarily commercial. Adding bi-directional capabilities to an EV increases cost, and it remains to be seen if enough consumers can be persuaded that it's worthwhile.

There is also an unresolved issue regarding who bears the cost for the new infrastructure needed for V2G, particularly the systems required to convert between the alternating current (AC) used in the grid and the direct current (DC) used to charge and discharge the EV battery at roadside fast chargers.

Power companies prefer using AC bidirectionally to facilitate the seamless addition of stored energy into their grids. However, automakers are concerned about the costs of adapting vehicle electronics to meet the demanding technical and safety standards of the grid.

Some consumers have expressed concerns that the additional charge/discharge cycles from V2G may accelerate the wear and tear on their EV's battery, leading to additional costs. Additionally, there are concerns about the round-trip efficiency as AC electricity from the grid is rectified to DC, stored in the car's battery, discharged from the battery, inverted back to AC again, and delivered back to the grid – with each step resulting in power losses. Charging stations for EVs typically use AC for residential and home chargers, while DC designs are increasingly common for fast chargers at roadside locations.

Governments may intervene to make bi-directional charging compulsory, as demonstrated by California's proposed Senate Bill 233 [3] which sets a deadline of 2027 for most new EVs and chargers sold in the state to support bi-directional charging. However, such a process may be slow and cumbersome.

System demands for V2G

EV charging presents a complex technical challenge that encompasses various aspects, including communications, security, user interface functions, and power conversion. It requires the use of one or more microcontrollers (MCUs) that run physical layer (PHY) and application software. Communication standards utilised may include Wi-Fi, Bluetooth, or cellular, with devices like NXP's IW620 dual-band solution or its OL2385 RF transceiver for sub-GHz protocols [4] [5].

Ensuring bidirectional charging necessitates robust security systems in both chargers and vehicles, encompassing confidentiality and authenticity. Hardware-based security solutions, such as NXP EdgeLock SE05x/A5000 secure element, offer easily integrated options for system designers. To handle the complexity of keys and certificates, NXP provides EdgeLock 2GO, a fully managed cloud platform [6].

To expedite development, NXP provides an EV charging station development platform that enables rapid prototyping and system design [7]. This platform allows customers to swiftly load Azure RTOS-based application software onto NXP's i.MX RT1064 crossover MCU and securely connect the simulated EV charging station to the cloud.

Smart EV charging dashboard

In EV chargers, wide bandgap (WBG) semiconductors like gallium nitride (GaN) and silicon carbide (SiC) offer superior efficiency compared to silicon alternatives. This is particularly crucial in EV chargers. For instance, Renault and CEA recently introduced a new bidirectional. charger supporting V2G, claiming a 30% reduction in energy losses during conversion thanks to the implementation of WBG materials [8].

Conclusions

The journey to reach the current state of V2G has been long and challenging. However, the adoption of V2G technology remains slow. While cars like the Nissan Leaf and Ford F-150 Lightning support bi-directional charging, they still constitute a minority [9]. Notably, Tesla has consistently opposed or shown reluctance to support bi-directional charging [10].

However, looking toward the future, we can envision a more promising outlook. With the rapid increase in the number of EVs on our roads, the time is ripe for V2G technology. The necessary technical solutions are already available, the standards are well-defined, and the demand is growing. Therefore, we should anticipate a significant rise in the prevalence of V2G in the coming years.

This article is part three of a three-part series of articles. You can find part one and part two below: 

 

Find out more about Avnet Silica’s solutions for EV charging

About Author

Harvey Wilson, Technology Specialist Connectivity EMEA
Harvey Wilson

Harvey Wilson is a Systems Engineer Professional (Smart Industry) for Avnet Silica in the EMEA regio...

EV Charging: How V2G Benefits Drivers and Electricity Suppliers
EV Charging: How V2G Benefits Drivers and Electricity Suppliers
Related Articles
Engineers wearing high-vis jackets walk past solar panels in a field
The Technologies Transforming Energy Management and Storage
By Harvey Wilson   -   June 24, 2025
The demand for electric energy surges, renewable sources like solar and wind are increasingly integrated into grids.
Alexander Battery Technologies logo
Forging Ahead: A Partnership Driving Innovation in Battery Technology
By Avnet Staff   -   June 24, 2025
In the dynamic world of electronics design and manufacturing, collaboration is often key to navigating complexities and seizing opportunities.
EV Charging: How V2G Benefits Drivers and Electricity Suppliers
Related Events
Next gen usb-c power
USB-C: The Smarter Power Solution
Date: February 26, 2025
Location: online, on-demand
Unlock Power Efficiency with onsemi
Date: December 10, 2024
Location: online, on-demand
Related Designs Menu