Manufacturing & Development Showroom

Fraunhofer Institute FEP
Making a thinner glass
Researchers at the Fraunhofer Institute FEP are teaming up with Corning, an American manufacturer of glass and ceramics, to create ultrathin glass for sheet-to-sheet and roll-to-roll processes right through to application in organic electronics. Ultra-thin glass can be used as a substrate as well as for encapsulation in many smart products such as Smartphones, curved displays, OLED light sources and photovoltaics. Especially appealing is to use ultra-thin glass in wearable electronics as well as in intelligent micro-optics and touch-sensors. Moreover, ultrathin glass has excellent surface properties that considerably exceed the ones of conventional plastic films.
Liebherr
Smart Construction Trucks

BigRep
LWorld‘s lrgest FDM 3D printed drone

University of Illinois
Revving up fiber networks
Need for speed: Milton Feng (r.) and his team are pushing the envolp for fibre (). cable
A team from the University of Illinois has successfully transmitted errorfree data at a rate of 57 gigabits per second (Gbps) through a fiber cable, thus creating a fast lane on the information superhighway. According to professor Milton Feng, the new technology, which is based on a special semiconductor laser, can operate at temperatures of up to 85 degrees, eliminating the need for additional cooling in hi-speed fiber networks. As big data has gotten bigger, the need has grown for a high-speed data transmission infrastructure that can accommodate the ever-growing volume of bits transferred from one place to another. Computing components grow warm over extended operation, as anyone who has worked on an hot laptop knows. Achieving high speeds at high temperatures is tricky Feng admits. Besides, cooling systems cost money. Latin America are squeezing out weaker players and reducing profit margins of those that remain.

Sign up for the Avnet Silica Newsletter!
Stay up-to-date with latest news on products, training opportunities and more!

Take a DEEP look into the future!
Get the latest market trends and in-depth trainings on our Digital Event Experience Portal!

Avnet Silica Design Hub
Browse and review hundreds of proven reference designs to accelerate your design process. Our designs can be modified and saved in our AVAIL design tool and then exported to your CAD tool of choice.