Custom Meta Tags
AVS Security Hero Banner
Sub Navigation
Avnet Silica Provisioning Service Title (MT)

Avnet Silica Provisioning Service

Avnet Silica Provisioning Service main content (LC)

Securing the production and logistics side of connected embedded devices is essential to good security practices. These threat vectors can be addressed using a provisioning service.

Security Provisioning - illustrated hub and nodes

 

The risk of unprotected manufacturing potentially exposing device credential during manufacturing is increasing. This can result in counterfeit products, reliability issues, low performance and quality, which leads to increasing warranty cost, and in worst case, undermine a company’s entire business case.
Avnet Silica has developed a highly secure solution for provisioning electronic components to cover the security in supply chain and distribution parts of electronic device manufacturers and OEMs.

The service offers a toolbox including everything customers need to set up a supply network, where secret information is never exposed, and always treated encrypted in a secure and documented process.

This service offers secure provisioning of devices through state-of-the-art encryption in a secure facility. Taking advantage of Avnet Silica’s flexible logistics setup.

ALS_Warehouse Locations_Poing

Warehouse

Poing (Germany)

Avnet Logistics are specialists in handling electronic components, providing ESD protection and operating quality-management systems based on ISO 9001, EN61340-5-1 & 2, ISO 14001 and J-STD020 & 033.

The Logistic Center in Poing is certified according to EN9120 and demonstrates its conformance to aviation, space and defence industry standards. EN9120 specifies additional management system requirements towards quality, safety and reliability within the supply chain of the Aerospace industry. This includes the chain of custody, traceability, stock control and availability of records.

Poing Warehouse (LC)

The warehouse Poing 1 has a total storage area of 27.500m² with 157.000 stock locations in the shelf area and another 12.000 locations in the pallets area.

The warehouse Poing² was built in 2011. The warehouse consists of a total area of 32.000m² (expanded by 7.500m²) with 289.000 storage locations in the shelf area and additional 45.000 locations in the Autostore.

ALS_Warehouse Locations_Autostore (MM)

The Autostore

The Autostore is a unique worldwide-patented warehouse system proven to be the ideal small-goods handler. With standardised boxes stacked in a cube, it is the most space-efficient goods-to-man system on the market. Besides that, there are 31.000 storage locations in the pallet area. The warehouse also features a sequencer, whose task is to collect all the individual items of orders and shipments, sort, store, save and perform together. The sequencer's performance is far above the current industry standard: twelve independent shuttles in three equally independent lanes allow 1200 called games per lane. Sufficient for each job density and a significant relief for picking.

Logistics PMC Intro (MM)

Product Modification Center

With a capacity to program over 40 million units and to tape and reel 45 million units, Avnet Logistics in Poing (Germany) currently operates the largest product modification center in Europe. The Avnet Logistics facility is certified according to DIN EN ISO 9001, DIN EN IEC 61340-5-1 & 2 and ISO 14001 meets high quality standards of the automotive, naval, aviation, aerospace, telecommunications, military and medical equipment industries.

Read More
OEM-ODM-EMS premises (LC)

Secure provisioning at OEM-ODM-EMS premises

Avnet partners with Trusted Objects to provide OEM-ODM-EMS with a fully integrated secure provisioning solution , adding to any existing programming equipment or test bench, secure provisioning and secure programming capabilities.

The product, called “tops plug&go” is based on a secure box connected to the programmer which ensures a full and secure control of the production with the following features:

  • Protect all sensitive data (application firmware, secrets) during the transit and during manufacturing operations, up to the programmable component
  • Generate and store securely in production, keys and certificates with the secure box’s HSM (Hardware Security Module)
  • Enable secure keys and certificates injection in the component and secure provisioning of the application server
  • Interface with factory PKI or external PKI
  • Compatible with most microcontrollers and most programming equipment or test bench

 

“tops plug&go” benefits

  • Automate and secure provisioning at OEM-ODM-EMS factory
  • Management of a proprietary PKI
  • Simplify certificates and keys generation at production site
  • Add value to IoT devices with a unique and strong “factory identity” per product
  • Matter-compliant security at factory: device initial certificate (DAC) secure generation and secure injection in MCU or electronic board
  • Protect software IP and credentials against illegal copies and cloning
  • Control the right number of provisioned devices with a trusted batch report
  • Deployed rapidly in any factory (full support from Trusted objects at the setup)

 

 

Realted Links

Related Links

 

Security Spotlight (GBL)

Device Management & Provisioning

When you are expanding security coverage to connected devices, Avnet Silica will help you with the challenge of designing security schemes complying with both Information Technology (IT) and embedded hardware standards.

Secure Provisioning Whitepaper (GBL)

Whitepaper

Secure Provisioning

Securing the production and logistics side of connected embedded devices is essential to good security practices. These threat vectors can be addressed using a provisioning service. Find out more on that topic in our whitepaper.

Security Services PDF (GBL)

Literature

Secure Provisioning Capabilities

Main stake of IoT Security - IoT Security implies the use of good practices in term of products, developments but it implies also to reduce opened doors, and provisioning is one of them.