Empowering the Smart Home Revolution: The Matter Standard
In an era where connectivity and convenience dominate consumer expectations, the smart home concept has rapidly evolved from a futuristic fantasy to a tangible reality. Yet, amidst the plethora of smart devices flooding the market, a significant challenge persists: compatibility. Consumers often encounter frustrating barriers due to disparate standards and protocols as they seek to integrate various smart products into their homes. Recognising this hurdle, the Connectivity Standards Alliance (CSA) introduced Matter, an ambitious initiative poised to revolutionise the smart home experience.
An Introduction to the CSA and Matter
The CSA believes that the Internet of Things (IoT) should positively transform the way we live, work and play. However, since the beginning, complexity, closed ecosystems and the challenges of accessibility, security and trust have held back progress in the way that the IoT has developed. Since 2002, when formally known as the Zigbee Alliance, the CSA has been dedicated to unravelling these challenges. Its goals are to simplify the complex, create an open path to IoT adoption and innovation, and promote universal open standards, enabling all devices to securely connect and interact with each other.
With a rich history of technology expansion, including the standardisation of Zigbee and later on Zigbee 3.0 with enhanced security features, the CSA has sort to develop a common language for smart devices. Dotdot, which was introduced in 2019, enables devices to speak to each other effortlessly on any network and forms the basis of Matter. Although the CSA is still responsible for Zigbee – Zigbee R23 was recently introduced with new features.
The companies responsible for running the CSA include Amazon, Google, Nordic Semiconductor, NXP Semiconductors, and STMicroelectronics to name but a few.
Walter Puhl talks through the Matter demonstration at Embedded World 2024
Since changing its name from the Zigbee Alliance, the CSA has become a multi-standards group enabling global collaboration across IoT players, accelerating market growth and delivering value to its members, the industry, and, most importantly, consumers. Primarily, the CSA is involved with standards development, which are delivered via a robust testing and certification program. With over 6,100 individual members representing 600 engaged companies, the CSA now has a total of seven Working Groups covering Matter, Health & Wellness, Access Control, Data Model, Product Security and Data Privacy, as well as Zigbee.
The Matter Working Group is responsible for the new universal IP-based standard Matter. It contains three sub-groups – Technical, Certifications, and Marketing & Product – which bring together the specification: and open-source software development kit (SDK), test tools, certification program and brand awareness. At its core, Matter aims to simplify the smart home landscape by providing a universal standard that promotes interoperability, security, and ease of use across different devices and platforms. Gone are the days of compatibility concerns, as Matter-certification assures end-users that they can seamlessly mix and match devices without worrying about integration issues.
One of the key strengths of Matter lies in its utilisation of existing networking technologies. By leveraging familiar protocols such as Wi-Fi, Ethernet, and Thread, Matter-compatible devices can seamlessly integrate into the home network without the need for specialised infrastructure. Moreover, the possibility of Wirepas integration opens up new avenues for enhanced connectivity and scalability, promising even greater flexibility and reliability in other smart home deployments like metering.
How does Matter work?
As previously discussed, Matter is IP-based: all of the commands that we interact with inside the Matter specification are above the transmission control protocol (TCP) and user datagram protocol (UDP) layers.
Matter is a common application layer – the languages of the IoT that helps smart device manufacturers develop interoperability with simplified set-up and control for those devices. The standard device types that are supported today include electrical smart bulbs, switches and plugs, blinds and shades, HVAC controls, smart TVs, access controls like door locks, safety and security systems, bridges and routers, and other controllers in a variety of different devices. As the Matter standard grows and develops, future areas could include smart healthcare, smart buildings and, even, smart cities.
Again, since Matter is IP-based, for command and control the standard supports Wi-Fi, Thread, Bluetooth Low-Energy (Bluetooth LE) for pairing purposes only, Ethernet and additional future network layers, like Wirepas. All with low overheads, for simple smart device types all you need is MCU-class compute power with less than 128KB RAM and 1MB Flash.
Zigbee, which is a 20-year-old full stack technology, is not IP-based like Matter but is 802.15.4 based. Thread is much like Zigbee as it’s 802.15.4 based but is an IP bearing technology. The Matter data models are basically the same as Zigbee and Thread, using the same definitions of a lightbulb or thermostat, for example.
Fortified security measures
In an age where privacy and security are paramount concerns, Matter places a strong emphasis on built-in security features. Through robust encryption and authentication mechanisms, such as the 10 specific areas outlined by the Connectivity Standards Alliance’s (CSA) cybersecurity requirements and recommendations, Matter ensures that user data remains protected against potential threats or breaches. This commitment to security instils confidence in consumers, fostering trust in the smart home ecosystem.
One aspect of security is device attestation, which is the Matter standard requires that every device type has a device attestation certificate (DAC). This certification requires a Product Attestation Authority (PAA), which provides attestation services to Matter devices, to ensure that each DAC is legitimate and meets the requirements of the Matter specification.
Attestation uses a public key infrastructure (PKI) that uses Root Certificate Authorities and Product Intermediate Certificates. This process is referred to as the Device Attestation Certificate Chain.
During the development and testing phases of the product, the manufacturer can test the device without the full attestation process. But once the device is in production phase, the all attestation requirements are enforced.
Looking for smart IoT and Device Security Solutions? See also:
- Secure Device Management and Provisioning
- Cyber Resilience Act Compliance Support and Solutions
- Software Security
We Talk IoT Podcast - Episode 39: Unified, Scalable, Secure - The Matter Promise for Enterprises
In today's dynamic B2B landscape, connectivity, interoperability, and scalability aren't just buzzwords – they're prerequisites for success. Enter Matter: a groundbreaking smart home standard, set to redefine how businesses approach IoT and smart technology.
Today, we have the privilege of hosting Guylain Pouly from NXP. We'll be diving into how Matter is shaping the business ecosystem, the opportunities it brings to the table for enterprises, and what its adoption could mean for the future of smart tech integration.
Pioneering smart home solutions
At the forefront of the Matter revolution is Avnet Silica, a trusted provider of innovative semiconductor solutions. Leveraging its expertise and industry partnerships, Avnet Silica empowers customers to navigate the complexities of the Matter ecosystem, from design conception to mass production and beyond. With a focus on confidentiality, integrity, and authentication, Avnet Silica ensures that smart home devices built on Matter standards meet the highest standards of quality and security. As a centre of expertise in Matter, Avnet Silica serves as a valuable aggregator of services and tools provided by suppliers - NXP Semiconductors, STMicroelectronics, Nordic Semiconductor, and Renesas - facilitating seamless integration and deployment of cutting-edge smart home solutions.
NXP Semiconductors
Secure Platforms & Wireless Solutions
NXP provides scalable, modular, and secure platforms to accommodate the diverse use cases Matter addresses - from end nodes to gateways - allowing device manufacturers to focus on product innovation and accelerating time to market. The i.MX Linux board support package (BSP), for example, includes Matter, Thread, and Border Router via a Yocto cross-compile recipe that works with all devices (i.MX 9, i.MX 8, and i.MX 6) supported by the most recent Linux BSP.
EdgeLock 2GO
In addition, EdgeLock 2GO is a CSA-approved PPA device attestation certificate issuer for Matter. EdgeLock 2GO, NXP’s service platform for provisioning and managing IoT devices, lets you securely install keys and certificates into your devices, either during manufacturing or in the field, and then keep credentials up to date during the device lifecycle. EdgeLock 2GO leverages the security capability of each device, for optimal levels of security across your entire IoT fleet.
Learn moreSTMicroelectronics
The STM32 MCUs bridges Matter to any other technology like Zigbee. Many IoT devices support Zigbee and will now also enable Matter. Supporting such type of dual infrastructure requires a solution able to bridge the communication between Matter-based device and Zigbee-based devices. The bridge device usually integrates high-performance MCUs with Ethernet capability to link connectivity products to the cloud. The dual-core STM32H7 MCU, for example, offers the right features to address this role, as it can embed the Matter layer and translate it into the Zigbee protocol and vice versa. The STM32WB wireless MCU, on the other hand, is ideal for Matter networks because it can run concurrently Thread and Bluetooth® LE used for device commissioning. The company provides two STM32 example projects. One demonstrates a Matter device over Thread and a gateway in RCP mode implemented on the STM32WB, while the other showcases how to create a Matter to no-Matter technology bridge based on the STM32H7.

Nordic Semiconductor
As one of the first company’s to receive a Thread 1.3 certification badge, Nordic Semiconductor offers this badge to its customers for their Thread products and is a prerequisite for Matter over Thread. Also, as a main contributor to the OpenThread stack, this combined with the company’s knowledge and experience in Bluetooth LE makes it an ideal partner to start developing new applications. The nRF54H20 ultra-low power SoC has multiprotocol radio covering Bluetooth LE, LE Audio, Bluetooth mesh, Thread, and Matter. The nRF54L15 is a next-level multiprotocol SoC with advanced security features.

Technology
Wirepas
Wirepas focuses on the wireless massive internet-of-things (IoT) connectivity, and the technology connects today around 10 million devices in many applications, including smart metering, smart building, smart tracking and smart manufacturing.

Evolving and extending Matter’s reach
Recognising the prevalence of existing smart home devices, Matter also prioritises backwards compatibility. Through software upgrades and bridge devices, legacy products can seamlessly integrate with the Matter ecosystem, extending their lifespan and enhancing their functionality. This commitment to inclusivity ensures that early adopters and long-time enthusiasts alike can reap the benefits of Matter’s universal standard.
Matter 1.2 came out recently, which begins to add a number of new device types like appliances (white goods), robotic vacuum cleaners, smoke detectors, energy management for EV charging, and doorbells and cameras. The belief is that Matter as a unified enabling technology of smart homes and smart building of the future that energy management is an opportunity for the standard to grow and really make a difference in society.
Many countries are uncertain what their future energy needs will be and how to reduce consumption. Connected technologies like Matter could provide invaluable to resolving both of those uncertainties. As more devices are digitalised or electrified, energy demand will initially increase but with better sensors we could know that if a room is empty for example to turn off the lights and not to heat it or cool it as much. There are a lot of other use cases that can be put into place with that focus on energy management.
With its commitment to compatibility, security, and innovation, Matter is poised to redefine the way we interact with our homes, ushering in a new era of convenience and connectivity. As industry leaders unite behind this groundbreaking standard, the future of the smart home has never looked brighter.
Overview
Smart Home & Smart Building Overview
Whether you’re developing a smart-home appliance or a system to control all of the functions in a commercial building, you need a partner who understands the associated standards, security aspects and data models. We helped create these standards.