DRAM芯片

DRAM (Dynamic random-access memory) is a type of random access semiconductor memory which is a volatile memory (meaning that its data is lost when power is turned off) and stores each bit of data in a separate tiny passive electronic component (such as capacitor) inside an integrated circuit. DRAM usually consists of one capacitor and transistor per data bit. Each electronic component has two states of value in one bit called 0 and 1 (like capacitor can either be charged or discharged; these two states are generally considered as 0 and 1). The capacitor starts to discharge slowly if there is no intervention, so the data on the chip also fades with the discharge. Capacitor need to be refreshed frequently to prevent this discharge so an externa refreshing circuit is needed to restore them to their actual charge and rewrite the data. Because of this frequent refreshing activity it is called as a dynamic memory. DRAM is used for frequent access and temporary data storage. DRAM is widely used where low-cost benefits and high-capacity memory is required. DDR (Double Data Rate) memory is the most commonly used DRAM memory and DDR4 is the latest generation of DDR. Also LPDDR is used for applications such as mobile and embedded boards where low power is concerned
DRAM芯片 Products under 存储器

有货时通知我

请登录/注册一个帐户,以便在有库存时通知您。如果您需要帮助,请联系在线支持.
sign in register

一般支持

+86-755-2184 5922 / +852-3129 9798

物料清单上传

请先登录以便上传物料清单
Add To Bom
该项目将被添加到您的“精确匹配”
关闭
显示   个产品
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
您需要登录才能查看内容
Add To Bom